{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the NEMA rating or IP degree of protection for door mounted S29338 and S29340 rotary handle operators for the Powerpact H and J breaker?
Product Line:
Circuit Breaker Accessories

Resolution:
S29338 and S29340 are IEC style, door mounted rotary operating handles. The handle mechanism can be used in NEMA 12 enclosure applications. Degree of protection: IP40 as per IEC 529.

Schneider Electric USA