{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the acceptable wire size range for the termination points on the Class 8903 Type SX lighting contactor?
Issue:
Checking the wire range for the 8903 SX Lighting Contactors

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8903 Type S Lighting Contactors

Resolution:
Power wiring: One aluminum or copper conductor #4 to 600 MCM (kcmil) or two #0 to 250MCM [kcmil].
Control wiring: #16 to #12 AWG copper.

Schneider Electric USA