{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do we have a DIN-rail mounted GFI breaker (4-6 mA trip)?
Issue:
Do we have a DIN-rail mounted GFI breaker?

Product Line:
QO-GFI breakers

Resolution:
No, there is no QOU-GFI version available. Suggested alternative is a QO-GFI breaker and an OEM mounting base such as a QON2L40. These bases are NOT DIN rail mountable, but they are an alternative to a large panel interior.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.