{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the part number for a replacement load side fuse base for a fusible bus plug ( 30 amps to 200 amps )?
Issue:
What is the part number for a replacement load side fuse base for a fusible bus plug (30 to 200 amps)?

Product Line:
I-Line busway fusible plugs

Environment:
Maintenance

Cause:
Replacement

Resolution:
Only the load side fuse base is available as a replacement part. See below for correct part number.

AMP SYSTEM SERIES PREFIX ITEM DESCRIPTION PART NUMBER
30 AMP 3W 4 PQ3203G LOAD BASE ASS`Y 240V 45201-590-50
30 AMP 4W 4 PQ4203G LOAD BASE ASS`Y 240V 45201-590-50
30 AMP 3W 4 PQ3603G LOAD BASE ASS`Y 600V 45201-623-50
30 AMP 4W 4 PQ4603G LOAD BASE ASS`Y 600V 45201-623-50

60 AMP 3W 4 PQ3206G LOAD BASE ASS`Y 240V 45201-623-50
60 AMP 4W 4 PQ4206G LOAD BASE ASS`Y 240V 45201-623-50
60 AMP 3W 4 PQ3606G LOAD BASE ASS`Y 600V 45201-624-50
60 AMP 4W 4 PQ4606G LOAD BASE ASS`Y 600V 45201-624-50

100 AMP 3W 4 PQ3210G LOAD BASE ASS`Y 240V 40520-216-50
100 AMP 4W 4 PQ4210G LOAD BASE ASS`Y 240V 40520-216-50
100 AMP 3W 4 PQ3610G LOAD BASE ASS`Y 600V 40520-216-50
100 AMP 4W 4 PQ4610G LOAD BASE ASS`Y 600V 40520-216-50

200 AMP 3W/4W 5 PS_____G LOAD BASE ASS`Y 240 & 600V `PS` 45201-229-50
200 AMP 3W/4W 5 PQ_____G LOAD BASE ASS`Y 240 & 600V `PQ` 45201-229-50

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: