{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do the Everlink contactors include 1 normally open and 1 normally closed aux contact as standard?
Issue:
Clarification on what auxiliary contacts are built in to the contactor

Product Line:
Contactors and Starters

Environment:
IEC contactors

Resolution:
The Everlink contactors includes 1 normally open (1 NO) and 1 normally closed (1 NC) auxiliary contact

Schneider Electric USA