{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is an NQ panel available with single bus construction for 120V and neutral only?
Issue:
NQ panel with single bus construction for 120V and neutral only

Product Line:
Panelboards.

Environment:
Products sold and used in North America

Cause:
Selection.

Resolution:
Yes. A single phase panel is available with both L1 and L2 buses tied together as factory assembled and UL approved as such. In Product Selectors, customer must use notes to engineering to obtain a through feed bus panel and Peru will cable between the through feed lugs, making all breakers at the same potential. Will be labeled properly as a UL listed 120V panel.

Schneider Electric USA