Search FAQs
Is Motorpact switchgear Service Entrance rated?
Issue:
Application, Codes/Std/Certification
Product Line:
INMVE - MV EQUIPMENT
Environment:
NEMA ICS 3, UL347, EEMAC G14-1, ANSI C19.7, IEC 60470, IEC 60529, IEC60694, IEC60129, IEC62271-102, IEC 62271-200, ANSI C37.20.7
Cause:
The NEC requires the electrical equipment which is used to connect a consumer of electric power to the utility source to be rated for Service Entrance.
Resolution:
Motorpact switchgear does not meet the requirements to be labeled as Service Entrance switchgear.
An incoming HVL or HVL/cc main switch can be added to meet this requirement.
CTA-ID : 2049927
Application, Codes/Std/Certification
Product Line:
INMVE - MV EQUIPMENT
Environment:
NEMA ICS 3, UL347, EEMAC G14-1, ANSI C19.7, IEC 60470, IEC 60529, IEC60694, IEC60129, IEC62271-102, IEC 62271-200, ANSI C37.20.7
Cause:
The NEC requires the electrical equipment which is used to connect a consumer of electric power to the utility source to be rated for Service Entrance.
Resolution:
Motorpact switchgear does not meet the requirements to be labeled as Service Entrance switchgear.
An incoming HVL or HVL/cc main switch can be added to meet this requirement.
CTA-ID : 2049927
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: