{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is a two pole, 100% rated PowerPacT P frame breaker available?
Issue:
100% application of a Powerpact P-frame Circuit Breakers

Product Line:
Molded Case Circuit Breakers

Resolution:
The two pole P frame breakers are not 100% rated. Use a 100% rated three pole breaker for the application and use two of the poles.

Schneider Electric USA