{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the replacement coil cover for an 8536 size 3 starter?
Issue:
Coil cover for an 8536 size 3 starter

Product Line:
NEMA Contractors and Starters

Environment:
8536 Type S Starters

Resolution:
If the device was made after January 1992, order 31074-054-01. If the device was made prior to 1992, the complete power plant assembly will have to be replaced.

Schneider Electric USA