How can we help you today?
What is the part number for mounting screws for Powerpact H and J frame circuit breakers?
Issue:
Powerpact H and J frame circuit breaker lug/lug mounting screws
Product Line:
Molded Case Circuit Breakers
Resolution:
The part number is 4820023650. It contains (2) 8-32 x 2-5/8" panhead screws. The breaker ships with these screws standard.
Powerpact H and J frame circuit breaker lug/lug mounting screws
Product Line:
Molded Case Circuit Breakers
Resolution:
The part number is 4820023650. It contains (2) 8-32 x 2-5/8" panhead screws. The breaker ships with these screws standard.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: