Part number for small pin on MCC that controls assembly is mounted to; it is at the edge of the bucket, and the plastic controls snaps onto it to hold it to the door
The CSP hinge assembly (on the left side of the CSP) is p/n 80401-851-50 The latch pin (the post on the right side of the saddle) is p/n 20490-30300, this will also need the pop rivet p/n 24303-63280
Released for:Schneider Electric USA
Explore more
Range:
Model 6 Motor Control Centers with AC Drives
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.