{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Several lighting contactors are shown in the catalog that are available to be built into Square D panelboards. What is the difference between the Square D and the ASCO offering?
Issue:
Several lighting contactors are shown in the catalog that are available to be built into Square D panelboards. What is the difference between the Square D and the ASCO offering?

Product Line:
NEMA Contactors and Starters

Environment:
NEMA Lighting Contactors

Cause:
Selecting a lighting contactor for a panelboard

Resolution:
Either type of contactor can be ordered interchangeably at the customer`s discretion. If the facility normally uses Square D products, they may want to be consistent and use the Square D contactors. This would simplify spare parts stocking, etc. Otherwise they can specify the Asco contactors.

Schneider Electric USA