Product Line:
Circuit Breaker
Accessory
Environment:
Electrical Distribution Equipment
Resolution:
Yes, the ELM150HD for the H frame breaker and ELM250JD for the J frame breaker provide 30 mA to 3 A sensitivity. The circuit breaker must have a 48 Vdc shunt trip. Suffix SP for factory installed or P29392 field installable.
NOTE: The ELM modules are for 3ph3w loads ONLY.
Circuit Breaker
Accessory
Environment:
Electrical Distribution Equipment
Resolution:
Yes, the ELM150HD for the H frame breaker and ELM250JD for the J frame breaker provide 30 mA to 3 A sensitivity. The circuit breaker must have a 48 Vdc shunt trip. Suffix SP for factory installed or P29392 field installable.
NOTE: The ELM modules are for 3ph3w loads ONLY.