{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What type secondary fuses are used in MCC starter units with control transformers? <br />What is the part number?
Issue:
Fusing for MCC buckets

Product Line:
Motor Control Centers

Environment:
Applies to MCC buckets by SquareD/Schneider Electric

Cause:
OverCurrent Protection for Control Transformers

Resolution:

Secondary fuses are FRN-R type fuses
120V 50VA CPT- .5 amp 25413-00060
120V 100VA CPT- 1.0 amp 25413-00090
120V 150VA CPT- 1.6 amp 25413-00130
120V 300VA CPT- 3.2 amp 25413-00190
120V 500VA CPT- 5.0 amp 25413-00230


Schneider Electric USA