Issue:
Selection and Maintenance
Product Line:
Motor Control Centers
Environment:
NEMA ICS 18-2001, EEMAC, UL 845, NFPA70 Art. 430
Cause:
Motor starters equipped with melting alloy or bimetallic overload relays require thermal units to operate.
Resolution:
Thermal unit selection charts are located in each motor control center sections's vertical wireway door.