Search FAQs
Is it possible to order panel skirts for the NQ or NF type panelboards for panels already installed in the field?
Issue:
Does Square D offer Is it possible to order panel skirts for the NQ or NF type panelboards for panels already installed in the field?
Product Line:
PTFDS - FD Enclosure Systems
Environment:
Panelboards and enclosures sold and supported in the USA.
Cause:
Is it possible to add a panelboard enclosure skirt to a panelboard already in the field?
Resolution:
Yes. To create a catalog number, use `PS` as a prefix added to suffix in inches, such as `PS21` for a 21`` panel skirt. Refer to pricing in the current Supplemental Digest.
NOTE: Panel skirts are for NEMA type 1 surface-mounted applications with standard depth and width, Square D™ brand enclosures ONLY.
Does Square D offer Is it possible to order panel skirts for the NQ or NF type panelboards for panels already installed in the field?
Product Line:
PTFDS - FD Enclosure Systems
Environment:
Panelboards and enclosures sold and supported in the USA.
Cause:
Is it possible to add a panelboard enclosure skirt to a panelboard already in the field?
Resolution:
Yes. To create a catalog number, use `PS` as a prefix added to suffix in inches, such as `PS21` for a 21`` panel skirt. Refer to pricing in the current Supplemental Digest.
NOTE: Panel skirts are for NEMA type 1 surface-mounted applications with standard depth and width, Square D™ brand enclosures ONLY.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: