{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What replaces the 3 pole 30 or 60 amp fusible switch base assembly, 40512-605-50, used in 8940N Series A and B pump panels?
Issue:
Are still available the switch base assembly used in 8940 Type N Pump Panels series A and B?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8940 Type N Pump Panels

Resolution:
Both the original switch base assembly 40512-605-50 and the replacement 40566-672-50 are now obsolete and no longer available.

Schneider Electric USA