{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: Do the current J250F and J250S NEMA Type 1, circuit breaker enclosures have provisions for a padlock to lock the breaker handle in the ON or OFF position?
Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosures

Resolution:
The J250S and J250F are provided with a padlock hasp as part of the front cover. The padlock hasp will enable a padlock to be used that will block the circuit breaker handle in either the ON or OFF position.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.