Search FAQs
What is the wire range for the 3 lugs in an AL1200P6KU kit?
Issue:
What is the lug wire range of the AL1200P6KU lugs and the dimensions of the wire binding screws?
Product Line:
Molded Case Circuit Breakers
Resolution:
Lug Wire range:
(3) 350-600 kcmil Al or Cu wires per phase
Wire binding screw dimensions:
Diameter: 15.4 mm
Length: 52.6 mm
What is the lug wire range of the AL1200P6KU lugs and the dimensions of the wire binding screws?
Product Line:
Molded Case Circuit Breakers
Resolution:
Lug Wire range:
(3) 350-600 kcmil Al or Cu wires per phase
Wire binding screw dimensions:
Diameter: 15.4 mm
Length: 52.6 mm
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: