{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the replacement control coil available for an 8910DPA42V06 Series B?
Issue:
8910DPA42V06 Ser B replacement coil

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8910DPA Definite Purpose contactors

Resolution:
9998DA1V06 (series B only), coil consumption is 56 VA inrush and 6 VA sealed.

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: