{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.

How can we help you today?

NQ 400A Main Lug Replacement

Issue:
Part Number for the replacement main lugs for an NQ 400A main lug panelboard interior

Product Line:
NQ panelboards sold and used in North America

Environment:
Maintenance/repair

Cause:
Can the main lugs be replaced on a 400A NQ main lug panelboard?

Resolution:
The replacement main lug part number, per lug is part number 80114-100-01.
This lug requires two mounting screws, part number 80114-001-05, one screw per part number.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: