{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a QO, 3 pole GFI, EPD, or EPE branch breaker be used in a QO403L100RB load center?
Issue:
Product Design Feature

Product Line:
QO 3-phase load centers and branch breakers

Resolution:
Yes, but only in current design, series G02, available since February of 2010. The series number can be identified on the package label or the device's wiring diagram. These breakers should not be used in any device with earlier series numbers.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: