{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What guard can be used with a ZB4BT4?
Issue:
Looking for a guard for ZB4BT4 operator

Product Line:
Pushbutton and Operator Interface

Environment:
Obsolete Product

Resolution:
Use a ZB4BZ2005 , ZB4BZ2105, or a ZBZ160* with cutout sides. Any of these will fit, however the padlocking feature will not work. These guards are made for the trigger action units, which are taller.

Schneider Electric USA