{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the replacement switch mechanism for a 9037HG12 and 9037HG32?
Issue:
Replacement switch mechanism for Class 9037 Type HG limit switches.

Product Line:
Pressure, Vacuum and Float Switches

Environment:
9037HG Float Switch

Resolution:
Switch Mechanism part number is 6507950251.  Orders for mechanisms must include the Class and Type so that the nameplate on the replacement can be correctly stamped.

Schneider Electric USA