{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are Square D MCCBs primary injection tested at the factory?
Issue:
Does Square D PI test molded case circuit breakers (MCCB) at time of manufacture?

Product Line:
Molded Case circuit breakers

Environment:
Testing

Resolution:
Square D Powerpact and the Masterpact NT and NW breakers are primary injection tested at the time of manufacture, to ensure they meet published trip curves.

Masterpact MTZ breakers are NOT high current primary injection tested at final assembly.  Sub systems like the CT's and control unit are tested at their respective manufacturing locations. The metering chain (CT to control unit) is verified using low current injection (around 200 amps) to verify metering on the HMI. Also, the control unit continuously monitors the health of the metering chain.


Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.