{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: What filler plate is used, and how does it install, to fill the main circuit breaker opening in a QO or Homeline, high amp, convertible main load center cover?
Issue:
Product Design Features

Product Line:
QO and Homeline Load Center

Resolution:
The High Amp (150-225Amp Max.) QO (Single phase ONLY) and Homeline load centers that use a QOM2 main breaker will use the filler plate part number QOM2FP.

The filler plate, QOM2FP is used on  the 150-225Amp load centers to fill the Main Breaker Opening for a QOM2 main circuit breaker.
The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.
A PDF copy of the complete instructions is attached below the video.


Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment. 
1) Once all Safety steps are followed, begin the installation of the Main breaker opening filler plate by following the instructions.
2) Install the filler plate (A) from the front of cover (B) by pressing into place as shown
NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric USA

Attachment(s)
QOM2FP instructions.pdf [60.71 KB]