Search FAQs
Are the EZM main fusible switch devices supplied with factory installed fuses?
Issue:
Product Design Features
Product Line;
EZM Metering
Resolution:
No. Fuses are not supplied factory installed and must be ordered and installed separately. EZM main fusible switches are configured for use with 300 Vac class T fuses in frame sizes of 400 A, 600 A, 800 A and 1200 A (Note: 1200 A is available in single phase only).
Product Design Features
Product Line;
EZM Metering
Resolution:
No. Fuses are not supplied factory installed and must be ordered and installed separately. EZM main fusible switches are configured for use with 300 Vac class T fuses in frame sizes of 400 A, 600 A, 800 A and 1200 A (Note: 1200 A is available in single phase only).
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: