{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do the Vario switches have 208V Horsepower ratings?
Issue:
Do the Vario switches have 208V Horsepower ratings?  If so, what are they?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Vario Switches

Cause:
Verify if Vario switches have 208V Horsepower ratings?

Resolution:
Yes, they do.

They are as follows:
Three phase, 3-pole 208V
V01 3 Horsepower
V02 2 Horsepower
V0, V1 5 Horsepower
V2 5 Horsepower
V3 7.5 Horsepower
V4 10 Horsepower
V5 20 Horsepower
V6 25 Horsepower

Schneider Electric USA