{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the HU364DS, series F5? (may be shown as F05)
Product Line:
Heavy Duty Safety Switch HU364DS, Series F5

Resolution:
The repair parts for the HU364DS, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base (all one piece) - 4056704050 - (1 required; includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 4020514202 (6 required per line base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - CL20F (includes 6 lugs - requires mounting screws below)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056678650 (also requires mechanism coupling assembly 40566-998-50 and interlock connector assembly 40567-188-50)
Switch Mechanism mounting screws- 2194900001 (2 required)
Handle Assembly - 4056736850
Lockplate - 4056738901
Lockplate mounting screws - 2194900001 (2 required)

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: