{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
MLN Panelboards and Replacement Circuit Breakers

Article available in these languages: Spanish

REVISION: The adapter kits listed below are now obsolete and no longer available. The Powerpact breakers do not have adapter kits available and cannot retrofit into the obsolete MLN panelboards. Consider replacing the panelboard with a new I-Line panel.

Issue:
Are replacement branch breakers still available for the obsolete MLN panelboards and switchboards from 1962 to 1968?

Product Line:
MLN panelboards and switchboards sold and supported in the USA through 1962 to 1968.

Environment:
Replacement breakers/maintenance.

Cause:
Are replacement branch breakers still available for the MLN product line:

Resolution:
The panel and breakers (ML) are obsolete. As 1/1/2015, we do offer adapter kits.

FAL and SK4515
KAL and SK4516
LAL and SK4517
MAL and SK4578

The best solution is to replace the complete panelboard and breakers with current products, see Digest 177, Section 9. Note that new panels will not be the same exact size as the older panels, and will likely be larger due to wire-bending space changes over the years. For assistance in selecting replacement products, first gather as many details as possible of the existing equipment. This includes information such as voltage, amps, interrupting rating, number and size of the circuit breakers, type of enclosure, etc. (the attached document below may help). Taking pictures of the complete panel with breakers may also help. Then, contact your local Schneider Electric authorized distributor, or you local Schneider Electric Field Office.

Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: