Issue:
What is used to connect the LTMR to the LTMEV relay?
Product Line:
IEC Contactors and Overload Relays
Environment:
TeSys T Motor Management Controller
Cause:
Installation
Resolution:
See the below cables.
Most commonly used is an LTMCC004 to tight couple them
What is used to connect the LTMR to the LTMEV relay?
Product Line:
IEC Contactors and Overload Relays
Environment:
TeSys T Motor Management Controller
Cause:
Installation
Resolution:
See the below cables.
Most commonly used is an LTMCC004 to tight couple them
2 x RJ45 | 0.04 (0.13) | |
0.3 (1) | ||
1 (3) |