Issue:
What lug is used for SL400?
Product Line:
Panelboards
Resolution:
This SL400 kit uses three of an AL400LA lug that accepts either (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 kcmil Al/Cu per phase.
What lug is used for SL400?
Product Line:
Panelboards
Resolution:
This SL400 kit uses three of an AL400LA lug that accepts either (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 kcmil Al/Cu per phase.