{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is the hanger and strain relief device included in the 9001BW?
Issue:
Identify if there's a hanger and strain relief device included in the 9001BW station

Product Line:
Type BW Pendant Station

Environment:
Push Buttons and Operator Interface

Cause:
Clarify if the strain relief needs to be ordered separately

Resolution:
Yes, strain relief and cord connector are now a standard features. The hanger is only available from the factory by adding Form Y236.

Schneider Electric USA