{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the Powerpact H and J frame breakers 100% rated?
Issue:
100% rated powerpact H and J frame breaker

Product Line:
Molded Case Circuit Breaker.

Environment:
Powerpact H Frame Breaker.
Powerpact J Frame Breaker.

Resolution:
100% rating is possible only with the following third digit termination codes: L, F, M, P, S. Suffix C would denote 100% rating on these breakers.
100% rating is not possible with following third-characters : A, N, D, K (I-Line, plug-in, drawout, I-Line with shroud on OFF end).

Schneider Electric USA