Issue:
8501KP Contact ratings
Product Line:
Relays and Timers
Environment:
Square D 8501 Type K Relays
Resolution:
Resistive 75% power factor continuous amperes: 10A.
At 240Vac, the 3 pole device has a 20A maximum total (sum of currents in all 3 poles), continuous rating.
8501KP Contact ratings
Product Line:
Relays and Timers
Environment:
Square D 8501 Type K Relays
Resolution:
Resistive 75% power factor continuous amperes: 10A.
At 240Vac, the 3 pole device has a 20A maximum total (sum of currents in all 3 poles), continuous rating.