{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the coil burden or draw on an EDB34020SA?
Issue:
What is the shunt trip's rated coil burden for a 120 Vac shunt trip on an EDB, EGB or EJB breaker?

Product line:
Molded case circuit breakers

Environment:
EDB, EGB and EJB circuit breakers for NF panel with a 120 Vac shunt trip

Resolution:
Max. current draw:  2400 mA
Coil burden:  288 VA
50 VA transformer recommended

Schneider Electric USA