{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for an H266AWK, series E2 heavy duty safety switch?
Issue:
Repair Parts for H266AWK Series E2

Product Line:
Safety Switch

Resolution:
The parts listed here are the only field replaceable parts that are still available.
Line base assembly - 4055221450SEL (2 required; arc suppressor assembly not included)
Load base assembly - 4055221550SEL (2 required)
Arc suppressor assembly - 4051270850 (2 required)
Lug assembly - 4025602450 (2 required per base assembly)
Line base phase insulator - 4051201401 (1 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250SEL
Vault handle - 4051219450SEL
Handle knob kit (black & red knob at end of handle) - 4401142750

Schneider Electric USA