{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for an H366AWK and H366NAWK, series E4 heavy duty safety switches?
Issue:
Repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4055218550SEL (3 required; arc suppressor assembly not included)
Load base assembly - 4055218750 (3 required)
Arc suppressor assembly - 4051270850 (3 required)
Lug assembly - 4405044601 (2 required per base assembly)
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (1 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217251
Vault handle - 4051219450
Handle knob kit - 4401142750
Solid Neutral Assembly - 4051269850 (can also use H600SN)

Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: