{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can you get ground fault trip and alarm with the Powerpact H, J, and L frame breakers with Micrologic trip units?
Issue:
Need ground fault alarm only
Product Line:
Molded Case Circuit Breakers
Resolution:
Ground fault trip comes with an LSIG trip unit. On a breaker with an LSIG trip unit, ground fault alarm can be obtained by adding suffix V on the breaker or by field installing the SDX module, S429532. Ground fault alarm only (without trip) is not possible on these breakers.

Schneider Electric USA