{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are EV Charging Stations UL or cUL Listed?
Issue:
Customer is looking for UL or cUL file information.

Product Line:
PTEVC - Electric Vehicle Systems

Resolution:
Level 2, 208Y/240 V stations are UL/cUL listed under File Number E338176.
Level 3, DC fast chargers are UL/cUL listed under File Number E474462.

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: