Issue:
Can the same EVRFIDHP (RFID handheld programmer) be used to program multiple EVlink chargers?
Product Line:
EV QUICK CHARGE EQUIPM
Resolution:
Yes. There is no limit to the number of EVlink chargers that the EVRFIDHP handheld programmer can be used to program.