Search FAQs
What is Included With the 31004-704-50 Parts Bag Kit for the 9421LJ7 Operating Mechanism?
Issue:
Breakdown of parts for the 31004-704-50
Product Line:
Operating Mechanisms for Circuit Breakers
Environment:
Type L Circuit Breaker Mechanisms
Resolution:
The kit has the following parts:
(1) Cotter pin part number 24201-08400 (not used)
(1) Toggle Extension part umber 29940-15540
(2) Mounting screws part number 22999-00041
Breakdown of parts for the 31004-704-50
Product Line:
Operating Mechanisms for Circuit Breakers
Environment:
Type L Circuit Breaker Mechanisms
Resolution:
The kit has the following parts:
(1) Cotter pin part number 24201-08400 (not used)
(1) Toggle Extension part umber 29940-15540
(2) Mounting screws part number 22999-00041
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: