{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do we offer a split bus options for an NF panel ?

Issue:
Split bus panel

Product Line:
Panelboards

Environment:
NF panelboards sold and supported in the USA.

Cause:
Interior layout

Resolution:
The NF is only available as 18-30, 30-18, or 30-30. There is no double split panel for NF.  Contact your local Schneider Electric sales office for further information on how to select and order this panelboard.

Schneider Electric USA