{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can I install a 200A subfeed breaker into a 400A NF panelboard?
Issue:
Can a 200A subfeed breaker be installed into a 400A NF panelboard?

Product Line:
NF Panelboard

Environment:
Application

Cause:
Add in the Field

Resolution:
A NF600SFBJ Sub feed Breaker kit would allow a J*L36200 circuit breaker to be sub fed out of the Panel, opposite end of the Mains.
Note: Back box size must be increased, refer to the NF panelboard section of the current Digest for box selection, see copy of Digest 178, pages 9-36 and 9-37, Tables 9.79 and 9.80  below:
Table 9.79 from Digest 178
Table 9.80 from Digest 178

Schneider Electric USA