{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do the NQ 14 inch wide interiors come in single phase?
Issue:
Are the NQ 14 inch wide interiors available in single phase?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
NQ panelboards sold and supported in the USA.

Cause:
Determination if NQ 14" wide panelboards are available in single phase.

Resolution:
Yes, single and three phase 14 inch wide NQ panelboards are available as Ready to Install. Refer to NQ panelboard section of current Digest  for selection.

Schneider Electric USA