{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are PowerPacT R frame, unit mount breakers available with lugs?
Product line:
Molded case circuit breakers

Resolution:
No, the unit mount version of the R frame is bus connected only.  For cable connections, you can order an RLTB (for all R frames other than 3000 A) or RL3TB (for 3000 A R frames only) terminal pad kit (one kit for each end of the breaker). These kits will take 8 or 9 lugs per terminal, respectively. You must use either the RLTB/RL3TB terminal pad kit or an equivalent UL listed terminal pad and bus structure in order to bring cables to this breaker.

Schneider Electric USA

Are PowerPacT R frame, unit mount breakers available with lugs?
Product line:  
Molded case circuit breakers

Resolution:  
No, the unit mount version of the R frame is bus connected only.  For cable connections, you can order an RLTB (for all R frames other than 3000 A) or RL3TB (for 3000 A R frames only) terminal pad kit (one kit for each end of the breaker). These kits will take 8 or 9 lugs per terminal, respectively. You must use either the RLTB/RL3TB terminal pad kit or an equivalent UL listed terminal pad and bus structure in order to bring cables to this breaker.

Schneider Electric USA
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
move-arrow-top