{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the largest size incoming conductor for the standard solid neutral on a NQ442L4C panel?

Issue:
Neutral lug size

Product Line:
Panelboards

Environment:
NQ Panelboards

Cause:
Wire selection

Resolution:
The standard 400 A  solid neutral aluminum mechanical lug can handle (1) 1/0-750 kcmil, or (2) 1/0-350 kcmil incoming conductors. Its is part # 80122-137-50.  The 200% rated solid neutral comes with two terminals with this same rating per each.

Schneider Electric USA