{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How many conductors and wire sizes will the AF2320GETBMB and CF2530GETBMB end tap box accept?

Issue:
Conductors and wire sizes accepted by AF2320GETBMB and CF2530GETBMB

Product Line:
I Line II Busway

Environment:
Wire size accommodation for termination

Cause:
Clarification regarding the minimum and maximum wire size that can be run to terminate to theAF2320GETBMB and CF2530GETBMB end tap boxes

Resolution:
The 2000A End Cable Tap Box will accept (7) 1/0-600kcmil conductors per phase.
The 3000A End Cable Tap Box will accept (10) 1/0-600kcmil conductors per phase and neutral.

This and other Busway  information can be found in the Busway Systems Class 5600 Catalog 5600CT9101

Schneider Electric USA

Attachment(s)
Busway 2012 Catalog 5600CT9101.pdf [8.75 MB]