{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do the XD4PA** Joysticks include the contact blocks?
Issue:
XD4PA12: Are the contacts included?

Product Line:
XB4/XB5 Specialty Operators Joysticks

Environment:
22mm Push Buttons

Resolution:
Yes the XD4PA joysticks include the contact blocks. It is provided with 1 normally open contact per direction.

Schneider Electric USA