Search FAQs
ATV312: What is the COS parameter?
Issue:
COS parameter in ATV312
Product Line:
Altivar
Environment:
Products sold and used in the United States
Cause:
NA
Resolution:
This is the Power Factor Parameter, located in the drC menu.
Look at the motor nameplate and use the power factor, typically designated as PF or COS. If no power factor is listed, use a value of .81.
CTA-ID : 2062182
COS parameter in ATV312
Product Line:
Altivar
Environment:
Products sold and used in the United States
Cause:
NA
Resolution:
This is the Power Factor Parameter, located in the drC menu.
Look at the motor nameplate and use the power factor, typically designated as PF or COS. If no power factor is listed, use a value of .81.
CTA-ID : 2062182
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: